cancel
Showing results for 
Search instead for 
Did you mean: 

Interfacing uPSD3253B to the databus of another microcontroller

info81
Associate
Posted on August 22, 2005 at 11:00

Interfacing uPSD3253B to the databus of another microcontroller

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
info81
Associate
Posted on May 17, 2011 at 12:08

I cannot figure out if it is possible to define a I/O-pin connected to the CPLD to act both as an input and as an output.

What I want to achieve is making it possible for another microcontroller (a Hitachi H8) to fetch and leave data to a port on the uPSD using the other controllers databus and the other controllers CE, RE and WE signals. In other words, combining a latch controlled by external WE with a buffer controlled by external RE on the same pin (letting the uPSD act as a type of memory to the H8).

Can anyone, with more experience with the uPSD than me, please tell me if this can be done?

jdaniel
Associate II
Posted on May 17, 2011 at 12:08

Magnus,

The best way to do this is to use a ''dual-ported RAM.'' This is basically a RAM chip with two separate address/data buses that connect to the same internal memory. They also have some arbitration and special registers that help the two processors coordinate their activies. Cypress Semi makes a pretty decent line of DPRAMs and I've used one of them successfully with a uPSD in a design.