cancel
Showing results for 
Search instead for 
Did you mean: 

I2C EEPROM with 10-bit address support

PrashantG
Associate II

Hi Team, I am looking for an I2C EEPROM (or any I2C slave device) that supports 10-bit addressing scheme. Can anyone suggest any device? 

Thanks,

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Super User

Here's one: https://www.ti.com/lit/ds/symlink/lm8330.pdf

via: https://www.ti.com/interface/i2c/general-purpose-ios-gpios/products.html 

So maybe worth a post on TI's forums to see if they have others: 

https://e2e.ti.com/support/interface-group/interface/f/interface-forum 

 

As the inventors & custodians of I2C, perhaps try asking on the NXP forums?

https://community.nxp.com/

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

6 REPLIES 6
Peter BENSCH
ST Employee

Welcome @PrashantG, to the community!

As far as I know, there are no EEPROMs with 10bit addressing. However, if it is to be any device, you can use any STM32 microcontroller, for example, where you can set addressing with 7bit or 10bit for slave operation.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Be more specific.

You want something supporting 10-bit I2C slave addressing?

Or you want an EEPROM with 1KB (8kbit) or more? You should be able to find 32KB (256kbit) EEPROM, that have a 7-bit I2C slave address, and then a 16-bit internal memory address.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes, I was looking for any device that supports I2C slave mode and 10-bit addressing. This is for evaluation of 10-bit I2C addressing scheme. 

I was preferring I2C EEPROM sort of device because I dont need to any programming of that device (Just power and access).  But as Peter mentioned, if nothing is available, i can check with STM32. 

Andrew Neil
Super User

Here's one: https://www.ti.com/lit/ds/symlink/lm8330.pdf

via: https://www.ti.com/interface/i2c/general-purpose-ios-gpios/products.html 

So maybe worth a post on TI's forums to see if they have others: 

https://e2e.ti.com/support/interface-group/interface/f/interface-forum 

 

As the inventors & custodians of I2C, perhaps try asking on the NXP forums?

https://community.nxp.com/

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

This is really helpful Andrew, Thanks a lot. 

You're welcome.

Please update with your findings from this "evaluation of 10-bit I2C addressing scheme"; as we've seen, it's not widely used - so some practical experience could be valuable!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.