cancel
Showing results for 
Search instead for 
Did you mean: 

HDD not in storage mgr

balaji_softproff
Associate II
Posted on October 04, 2006 at 05:34

HDD not in storage mgr

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
balaji_softproff
Associate II
Posted on September 01, 2006 at 03:10

Hi,

We are using stpc atlas reference board. We are able to boot windows CE 5.0 on it. The Bios used is from GS. The Stpc atlas BSP is used to build the NK.bin

The Bios when booting shows the Hard disk connected but after wince 5.0 loads there is no HDD in the storage manager. Can anyone help with this.

Balaji

kaouther
Associate II
Posted on September 01, 2006 at 06:20

Hi,

You should add an environement variable STPC_IDE0 set to 1 in the IDE storage setting. Attached a screen show how to add a new environment variable to the storage device setting .

________________

Attachments :

Variable-Setting.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtqJ&d=%2Fa%2F0X0000000aXi%2FXJ.HjoPbgpCsdUFs93IpKrEL5_zjqD8VAPOXNCkWZVI&asPdf=false
balaji_softproff
Associate II
Posted on September 04, 2006 at 07:46

hi,

Thanks for your previous reply

I am using wince5.0 platform builder. I don't know how to set the environment variable for storage devices. using the platform builder version 5.0. can U help me with this.

Thank you

Balsara

________________

Attachments :

test.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htsn&d=%2Fa%2F0X0000000aYJ%2F9yyRNrIjWUdeNJbK2z6WZ5KIoCeYblgEbC9G6qT9ZwY&asPdf=false
balaji_softproff
Associate II
Posted on September 04, 2006 at 10:25

hi,

I have booted WINCE5.0 with USB mass storage, Network card in PCI slot and Hard disk in IDE connector. Thanks for your help

Now working to get on with CDROM

Thanks

Balaji

balaji_softproff
Associate II
Posted on September 05, 2006 at 05:27

Hi,

In windows CE 5.0 I have connected harddisk as master and connected CDROM as slave. The hard disk shows up in the storage manager, But I could not find CDROM in it, can anyone help me with this.

Thanks

balaji

balaji_softproff
Associate II
Posted on October 04, 2006 at 05:34

completed wince with network,cdrom,harddisk and usb mass storage device.

going for slackware.

Is tinybios compatible in atlas evaluvation board

has anyone tried it

thanks

Balaji