cancel
Showing results for 
Search instead for 
Did you mean: 

framebuffer for stpc

gal
Associate II
Posted on March 12, 2003 at 09:32

framebuffer for stpc

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
gal
Associate II
Posted on March 11, 2003 at 08:02

Hello,

I have stpc Atlas evaluation board . I want to install framebuffer

on linux kernel. I download the framebuffer device from

http://www.stmcu.com/devicedocs-Atlas-75.html .

What linux kernel version do I need ?

I have red hat linux kernel version 2.4.18, Can I use this version?

thanks in advance.

thierry239955_st
Associate II
Posted on March 12, 2003 at 09:32

Linux drivers are more or less portable from one version of kernel to another. In most of case there is no modifications to be done and you just have to re-compile. In few cases, there is small adjusment to be done.

The best is you try and see if you get errors during the compilation.

As far as I know, in the 2.4.x series, no modifications have be done after the version 2.4.5 and you should be able to compile any 2.4.5 or later version with the same source code.