cancel
Showing results for 
Search instead for 
Did you mean: 

External SRAM troubles

bhines
Associate II
Posted on January 12, 2010 at 12:06

External SRAM troubles

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
bhines
Associate II
Posted on May 17, 2011 at 09:45

I have a 512k by 8 bit SRAM interfaced to an STR912FW44 via 8-bit multiplexed mode using CS0. Whenever I write a byte to it, it writes the same byte into 4 locations in the SRAM two bytes 10 hex apart in two places 100 hex apart. What am I doing wrong? The compiler is keil C.

sfouques9
Associate II
Posted on May 17, 2011 at 09:45

Hi All,

Does anyone found why CS0 is activated 4 times in 8bits (or even 16!!) mux mode when writing a single byte at a single location ??? I did not found any chronogram for this mode ??

With the same configuration on CS1, CS1 is activated correctly one single time ?!!

regards,

lxu
Associate
Posted on May 17, 2011 at 09:45

Do you define the SRAM address like this (*( volatile char*) 0x30000000)?