cancel
Showing results for 
Search instead for 
Did you mean: 

ESD EMI protection for USB OTG

koyala
Associate
Posted on March 16, 2016 at 10:20

Hello ,

As per my project requirement, i need to design USB OTG which meets the ESD standard IEC 61000-4-2 level 4) and EMI standard CISPR-11. 

In ST website i found two categories:

1. Common mode filter with ESD protection

2. EMI filter and ESD protection

Both claims, same ESD protection levels.

So, i am not sure which is used for what and what is the basic difference between them.? 

Kindly suggest.

Regards,

Govind.

#emi/esd #usb-otg
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Petr Ourednik_O
ST Employee
Posted on July 11, 2018 at 17:02

Hi,

To solve interference problems, you must understand them. So at first please begin by describing the ways

that RF interference is coupled into equipment and detected. There are several principal mechanisms

at work. You should study this tutorial thoroughly to understand how these things work.

http://audiosystemsgroup.com/RFI-Ham.pdf

http://www.karinya.net/g3txq/chokes/

Hope it helps,

P.