2007-10-16 9:38 PM
2011-05-17 12:47 AM
Andras,
Thanks for the tip. I got real excited and thought this might be it! But it looks like this is taken care of in the IRQ.s code.Code:
LDR R1, =VectorAddrDaisy ; Write to the VectorAddressDaisy to STR R1, [R1] ; clear the respective Interrupt Good thought though!2011-05-17 12:47 AM
Next tip:
What is the purpose of that endless while(1) ??? cheers, Andras2011-05-17 12:47 AM
Jsarao
I had same problem, on heavy traffic it suddenly stoped, no more interrupts. I take lot of code from Keil ENET driver and also modified, and now its works. First, Keil use its own software to handle descriptors, and I think it is a bug in ST software (version 1.1), the init routine of RX descriptor don't set the NPOL_EN bit on the last descriptor, maybe the problem is there. Here is my interrupt code void ENET_interrupt(struct netif *netif) { struct ethernetif *ethernetif = netif->state; int err = 0; u16 len; u32 i, j, int_stat, RxLen; u32 *sp,*dp; while((int_stat = (ENET_DMA->ISR & ENET_DMA->IER)) != 0) { /* Acknowledge the ENET interrupts. */ ENET_DMA->ISR = int_stat; /* RX interrupt */ if(int_stat & DMI_RX_CURRENT_DONE) { /* Valid frame has been received. */ for(j = 0, i = RxBufIndex; j < NUM_RX_BUF; j++) { /* Find it in the DMA Descriptor List. */ if((Rx_Desc[i].Stat & DMA_DSCR_RX_STATUS_VALID_MSK) == 0) { /* OK, a packet is found, check if any error */ if(Rx_Desc[i].Stat & DMA_DSCR_RX_STATUS_ERROR_MSK) { /* Error, free packet. */ err = TRUE; } /* Check frame length. */ RxLen = (Rx_Desc[i].Stat & DMA_DSCR_RX_STATUS_FLEN_MSK); if(RxLen > netif->mtu) { /* Packet length too big */ err = TRUE; } if(!err) { /* Valid packet, wake up input Thread */ if(!ethernetif->rxData) { // No pending inputs ?.. QPut(THREAD_LWIP, PRIO_NORMAL, EVT_RCV0, 0); } ethernetif->rxData++; // Coun up pending inputs } else { /* No valid packet, free packet. */ Rx_Desc[i].Stat = DMA_DSCR_RX_STATUS_VALID_MSK; } /* Count to next */ if(++i == NUM_RX_BUF) i = 0; } else { /* Count to next */ if(++i == NUM_RX_BUF) i = 0; /* Set next receive */ RxBufIndex = i; } } } /* TX interrupt */ if(int_stat & DMI_TX_CURRENT_DONE) { /* Frame transmit completed. */ for (i = 0; i < NUM_TX_BUF; i++) { if ((Tx_Desc[i].Ctrl & DMA_DSCR_TX_STATUS_VALID_MSK) == 0) { /* Release Transmited frames from DMA buffer. */ Tx_Desc[i].Ctrl = 0; } } } } /* Acknowledge the VIC interrupt. */ VIC0->VAR = 0; } The Qput function mails input to wakeup the input-thread and the thread moves data from descriptors to buffers in my system2011-05-17 12:47 AM
Hi
If you missing interrupt, also check spurious interrupt. you have to setup VIC0_DVAR = (u32)Default0_IRQHandler; VIC1_DVAR = (u32)Default1_IRQHandler; Search in forum for how todo