ENET DMA overflow on receive
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-10-16 9:38 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
Hi
I use Keil ethernet driver with lwip and have problem to handle receive overflow on DMA. I have enabled the RX_NEXT interrupt (generated if no valid descr found) and I also got the interrupt and trying to drop the packet by setting the VALID bit, but it not works, I got a new interrupt directly. Has anyone an example how to handle it in right way, maybe I have to go throu all descr and set the VALID bit ?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
What are you trying to achieve? Counting the dropped packets?
I don't now the KEIL driver, but the VALID bit should be set after you processed the packet. Until that packets are dropped automatically. Andras- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
First of all I will get it running without stop and drop the overflow packets.
To clearify, if I set the NPOL_EN it will drop the packet automatically and on RX_CURR_DONE I process the receive packet and set the VALID bit If all descr are occupied the packets is dropped, but do I still got RX_CURR_DONE for the queued descr so I can continue to process recive packets- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
you should have NPOL_EN=1 loaded from descriptor (ENET_RXNDAR) but also
NXT_EN=1 in ENET_RXCR loaded from DMA_CONTROL part of descripor (where DMA_XFERCOUNT = size is) NPOL_EN is for polling only, if you can guarantee that next buffer is always valid, or you restart fetching after an overflow NEXT_EN should be enough. This could save some cycles depending on DFETCH_DLY but is more complicated than just setting the VALID bit. Andras [ This message was edited by: alandras on 27-09-2007 13:51 ]- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
It works now, and it was necessary with the loop.
The driver use 4 descr for receive and 2 descr for send, maybe the performance is little slow, maybe the stack is the problem I have tested it with ping running and stop/run the board with debugger and the ping allways start again. Also tested with Netwox generating random IP block together with ping, and ping mostley timeout but still running. Thanks for all help- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
I have NPOL_EN as you describe and now it never stop, I also put in a loop in interrupt on RX_CURR_DONE to see if it is more than one descr ready, maybe this is not necessary ?
How can I counting dropped packets on easy way, shall I use RX_NEXT interrupt ?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
>>RX_CURR_DONE to see if it is more than one descr ready, maybe this is not necessary ?
I think so. >>How can I counting dropped packets on easy way, shall I use RX_NEXT interrupt ? There is a ''PACKET_LOST_EN: PACKET_LOST interrupt enable'' in the ''DMA Interrupt Enable Register'' and ''RX_TO_EN: RX_TO interrupt enable'' but is not well documented. Andras- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
Reference Manual
http://www.st.com/stonline/products/literature/um/12126.pdf page 98 Current Vector Address Register (VICx_VAR) ''– At the end of the ISR, write to the VIC0_VAR register (or VIC1_VAR if the interrupt source is from VIC1) to update the priority hardware.'' Could be this? Andras- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 12:47 AM
JW,
Do you have sample code of your Ethernet (ENET) Interrupt Handler routine that you can post? I think I'm having a similar problem: 1. Ethernet interrupts occur (RX_CURR_DONE) 2. Handle interrupt: copy data from descriptor, set valid bit 3. At some point later, I no longer get any interrupts PROBLEM: I never see any of the error interrupts (PACKET_LOST_EN, RX_MERR_INT_EN, RX_TO_EN) PROBLEM: I no longer get any receive interrupts either Here is my current handler (trimmed down):Code:
void ENET_IRQHandler(void) { while ( (ENET_DMA->ISR) & ENET_DMA->IER ) { // 15: RX_CURR_DONE_EN: RX_CURR_DONE interrupt enable if ( ENET_DMA->ISR & 0x00008000 ) { ENET_IRQ_COUNT[15]++; if ( ENET_HandleRxPkt( RCVR_BUFFER ) == 0 ) { while ( 1 ) { } } ENET_DMA->ISR |= 0x00008000; } } }