cancel
Showing results for 
Search instead for 
Did you mean: 

DMA and SSP1

hamouz
Associate
Posted on November 25, 2011 at 14:45

I would like to use DMA with SSP1. There is a problem that when flow control is set to peripheral, data are transfered, but I am not able to control how many bytes are transfered. If I change flow control to DMA, nothing happens. Any single transfer doesn't occur, although both single and burst requests are signaled (registers DMA_SSBR and DMA_SBRR).

I can't find where is the error. I believe I did my best according to documentation.

In previous topics there was an example (Example of DMA and SSP, 11/9/2006 2:10 AM), but the attachment is lost and no longer available. Eris, can you post it again?

Tomas

My code:

==============================================================

#define    SPI_SD               SSP1

#define    DMA_CHANNEL_RX       DMA_Channel4

#define    DMA_CHANNEL_TX       DMA_Channel5

#define    DMA_CHANNEL_RX_IDX   Channel4

void str91_dma_transfer_receive( const BYTE *buff, UINT count)

{

    DMA_InitTypeDef         DMA_InitStructure;

    WORD rw_workbyte[] = { 0xffff };

    DMA_DeInit();

    DMA_Cmd(ENABLE);

    // shared DMA configuration values

    DMA_InitStructure.DMA_Channel_LLstItm = 0;

    DMA_InitStructure.DMA_Channel_DesWidth = DMA_DesWidth_Byte;

    DMA_InitStructure.DMA_Channel_SrcWidth = DMA_SrcWidth_Byte;

    DMA_InitStructure.DMA_Channel_DesBstSize = DMA_DesBst_1Data;

    DMA_InitStructure.DMA_Channel_SrcBstSize = DMA_SrcBst_1Data;

    DMA_InitStructure.DMA_Channel_TrsfSize = count;

    // RX - storing data in buffer

    DMA_InitStructure.DMA_Channel_SrcAdd = (DWORD)(&SPI_SD->DR);

    DMA_InitStructure.DMA_Channel_DesAdd = (DWORD)buff;

//        DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl2_DMA;  // peripheral_to_memory / DMA

    DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl_Perip2;  // peripheral_to_memory / SSP

    DMA_InitStructure.DMA_Channel_Src = DMA_SRC_SSP1_RX;

    DMA_InitStructure.DMA_Channel_Des = 0;

    DMA_Init(DMA_CHANNEL_RX, &DMA_InitStructure);

    DMA_ChannelSRCIncConfig(DMA_CHANNEL_RX, DISABLE);

    DMA_ChannelDESIncConfig(DMA_CHANNEL_RX, ENABLE);

    

    // TX - must send 0xFF

    DMA_InitStructure.DMA_Channel_SrcAdd = (DWORD)rw_workbyte;

    DMA_InitStructure.DMA_Channel_DesAdd = (DWORD)(&SPI_SD->DR);

//        DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl1_DMA;  // memory_to_peripheral / DMA

    DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl_Perip1;  // memory_to_peripheral / SSP

    DMA_InitStructure.DMA_Channel_Src = 0;

    DMA_InitStructure.DMA_Channel_Des = DMA_DES_SSP1_TX;

    DMA_Init(DMA_CHANNEL_TX, &DMA_InitStructure);

    DMA_ChannelSRCIncConfig(DMA_CHANNEL_TX, DISABLE);

    DMA_ChannelDESIncConfig(DMA_CHANNEL_TX, DISABLE);       // reusing the same data in memory

    // enable interrupts

    DMA_ITConfig(DMA_CHANNEL_RX, ENABLE);

    DMA_ITConfig(DMA_CHANNEL_TX, ENABLE);

    DMA_ITMaskConfig(DMA_CHANNEL_RX, DMA_ITMask_ITC, ENABLE);

    DMA_ITMaskConfig(DMA_CHANNEL_TX, DMA_ITMask_ITC, ENABLE);

    // Enable  TX/RX request in SSP controller

    SSP_DMACmd(SPI_SD, SSP_DMA_Receive, ENABLE);

    SSP_DMACmd(SPI_SD, SSP_DMA_Transmit, ENABLE);

    

    // Enable DMA channels

    DMA_ChannelCmd(DMA_CHANNEL_RX, ENABLE);

    DMA_ChannelCmd(DMA_CHANNEL_TX, ENABLE);

    // wait for end of transfer

    while (DMA_GetITStatus(DMA_CHANNEL_RX_IDX, DMA_TCRS) == RESET);

    // Disable DMA channels

    DMA_ChannelCmd(DMA_CHANNEL_RX, DISABLE);

    DMA_ChannelCmd(DMA_CHANNEL_TX, DISABLE);

    // Disable  TX/RX request in SSP controller

    SSP_DMACmd(SPI_SD, SSP_DMA_Transmit, DISABLE);

    SSP_DMACmd(SPI_SD, SSP_DMA_Receive, DISABLE);

    DMA_Cmd(DISABLE);

}  // str91_dma_transfer_receive
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
DGuil
Associate

I am having this issue also. Im using a STR911FAx44. I know this post is old but I would like to see an asnwer. I am in the process of updating legacy firmware and would like to use the DMA. Interrupt does not fire until, what looks like the entire ram space is transferred. I am transferring to the UART in my case.