Skip to main content
nlovallo
Associate
August 12, 2011
Question

DFU and EHCI

Posted on August 12, 2011 at 15:52

Has anyone else had problems getting DFU to work over an EHCI (USB 2.0) host controller? When I perform an upgrade over an EHCI controller, the last packet of every transfer is corrupted.  If, on the same computer, I perform the same upgrade over an OHCI/UHCI (USB 1.0) host controller, the upgrade works fine.  If I trace the transfer at the kernel level using a tool like USBTrace or USBlyzer, all the packets look fine.

#dfu
This topic has been closed for replies.

3 replies

nlovallo
nlovalloAuthor
Associate
August 17, 2011
Posted on August 17, 2011 at 22:47

I have narrowed this down further and found that using the IAR Embedded Workbench compiler, if I disable optimizations, I experience problems when I download firmware.  The last 64 byte packet of every USB transfer seems to be corrupted.  If I set optimizations to 'High', everything works as expected.  Any experience or advice related to this problem would be appreciated.

Pantuca.Erwin
Visitor II
August 22, 2011
Posted on August 22, 2011 at 06:52

we can only conclude in general that without optimizations the code is too bloated/slow that may cause such problems.

nlovallo
nlovalloAuthor
Associate
August 23, 2011
Posted on August 23, 2011 at 17:53

I should have mentioned I am using ST's DFU example code, on an ST Eval Board, with ST's DFU Demo application. I guess I wouldn't expect such a simple example to have these kind of performance issues.  And it also seems to be a pretty specific ''performance problem'' that the last packet of every transfer is being corrupted.  Perhaps at the lower optimization level something is being initialized incorrectly...