cancel
Showing results for 
Search instead for 
Did you mean: 

Debugging with the ST7-STICK

wolfgang2399
Associate II
Posted on November 24, 2004 at 10:31

Debugging with the ST7-STICK

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
wolfgang2399
Associate II
Posted on November 17, 2004 at 13:03

Hi,

I use the ST7-STICK to programm my ST7FLite2x.

Reading the AN1754 I found that you can test the ST7-application under the ICC-protocol.

Has anybody of you experiences in in-circuit-debuggig via ICC protocol and the ST7-STICK. Or do you know a good software system ready to use? Can I include the STVD7 software and how?

Thanks for any idea,

WoRo

alain2399
Associate II
Posted on November 24, 2004 at 10:31

Hi Woro,

Unfortunatly the Stick does not support ICD (In Circuit Debugging). You have several hardware that supports ICD on the ST72FLite2x using STVD7 as IDE:

* InDart from Softec

* EMU3 from ST

* DVP3 (starting from STVD7 r3.1 to be released in December 2004).

As the ICC/ICD is open, you can expect other third parties to support it but not with STVD.

Alain