cancel
Showing results for 
Search instead for 
Did you mean: 

DEBUG Interface

jm2
Associate
Posted on November 25, 2003 at 18:33

DEBUG Interface

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jm2
Associate
Posted on May 17, 2011 at 11:57

Hi!

I'm designing a PCB with a µPSD3212 - but want to be able to put a µPSD3333 as an option.

A FLASH-Link Port for the µPSD is designed on the PCB. In addition to the µPSD3212 the µPSD3333 has a ''DEBUG''-pin.

What to do with this pin to be sure, that I can use the debugging-features? What external hardware do I have to use for debugging? I have the 3200 developement-board and the FLASH-Link-Interface for the printer-port. May I use this for a µPSD3333 as well? Will I be able to archive debugging-features with this?

Is there already a App-Note for the µPSD3333, that sums up the debugging-features?

Thanks very much![addsig]
joseph2399
Associate II
Posted on May 17, 2011 at 11:57

Please see the attached, AN1724 , Conversion Guide uPSD3200 to uPSD3300. Also attached, Application note AN1763, has a section on KEIL'S uLink USB-JTAG Debugger used on uPSD33xx.