cancel
Showing results for 
Search instead for 
Did you mean: 

Cosmic Compiler bug

burakakcasu
Associate II
Posted on August 12, 2008 at 10:22

Cosmic Compiler bug

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
burakakcasu
Associate II
Posted on August 08, 2008 at 08:34

Hi.

I'm trying to learn Cosmic Compiler program. For programming ST7 microcontrollers.

I have a problem about Compile and build.

I work with example program. I press compile or build button and i get this

error message

''Can't Access File:IDEABLD.BAT in Project Directory. Check Access Rights.''

I use Windows Vista as operating system.

Could you help me.

Thanks.

Burak Akçasu.

luca239955_st
Associate III
Posted on August 11, 2008 at 05:23

as the error message says, make sure you have full rights on the project directory. If you have no clue, log in as admin and try again.

Regards,

Luca (Cosmic)

burakakcasu
Associate II
Posted on August 12, 2008 at 03:59

Quote:

On 11-08-2008 at 08:53, Anonymous wrote:

as the error message says, make sure you have full rights on the project directory. If you have no clue, log in as admin and try again.

Regards,

Luca (Cosmic)

Thanks for your answer. But it didnt work. I have full rights on project directory but still i get same error message.

I think it is about Windows Vista.

Thanks again. I think i must return Windows XP :).

luca239955_st
Associate III
Posted on August 12, 2008 at 07:46

>> I think i must return Windows XP :).

probably a wise choice :)

However, of course, we have tested the compiler on Vista ans it does work.

Good luck.

Luca

burakakcasu
Associate II
Posted on August 12, 2008 at 10:22

thanks.

huayangflorida
Associate
Posted on May 17, 2011 at 15:31

Hi, I saw the posted problem but didn't see solution.

Could anybody help?

I work with example program. I press compile or build button and i get this

error message

''Can't Access File:IDEABLD.BAT in Project Directory. Check Access Rights.''

I use Windows-7 64bit as operating system.

xander2015
Associate II
Posted on January 12, 2012 at 02:27

you should use 32bit system.

wolfgang239955_stm1_st
Associate II
Posted on January 23, 2012 at 09:29

Hi,

I failed to start the Cosmic Compiler when residing the source files on our intranet. After I've transferred all my files to my local drive - there has been no problems any more.

Take it just as a suggestion,

WoRo