cancel
Showing results for 
Search instead for 
Did you mean: 

bug in stvd7

rob239955_st
Associate II
Posted on February 28, 2005 at 09:43

bug in stvd7

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
rob239955_st
Associate II
Posted on February 28, 2005 at 09:43

Hi

i don't know whether the following are a bugs or by design;

When using the debugger in stvd7 the various window positions and sizes are not stored, for example if i open the st7 register window and undock it, then resize it (as it does not need the whole screen width) then exit the debugger, when i go back into the debugger the left hand position seems to have been remembered but the window width is always set to the screen width.

This appears to happen with all windows, e.g watch, peripherals etc

Also when i exit the debugger and go back to the editor screens, the editor window is shown as focussed (top bar blue) but clicking on the main window menu item does not offer any windows as being open, this is refreshed when you click on the top bar of the supposedly focussed window)

I don't know whether the above are bugs or not - I would say the first one certainly is, any chance of sombody sorting this one?

thanks

rob carter