cancel
Showing results for 
Search instead for 
Did you mean: 

Bootloader on bank1 loads application to bank 0, But applic. can't run

hmehmetkurnaz
Associate II
Posted on September 26, 2007 at 11:48

Bootloader on bank1 loads application to bank 0, But applic. can't run

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
hmehmetkurnaz
Associate II
Posted on May 17, 2011 at 09:47

Hi all.

My bootloader on bank1 gets application from uart and loads to bank0.And i tried to jump my application with and without soft remap.But my application doesn't run.I have debuged for understanding what is happenning.I listed some problems.

1-

First off all when it is on bank1 hardware reset with reset

button(I use Keil MCB-STR9) doesn't reset cpu until push to reset

button second time.Also watchdog reset can't reset cpu

2-

flashBankRemap(0x00, 0x06, 0x80000, 0x0000);

// Jump to the user application and execute it

appfunction = (ApplicationStartup) 0x0000;

appfunction();

After appfunction(), PC loads 00 and on every step into command (debug)

PC increase 4 (0-4-8-c....).I would expect PC first loads 0 and than

Reset_Handler(in my prog 0x58).In your opinion can that be a problem.

In this state soft remap is ok because after reset bootloader doesn't

run.

3-

appfunction = (ApplicationStartup) 0x80000;

appfunction();

If i don't soft remap and just jump to 0x80000, PC loads with 4;

it should be error because PC has to be loaded with 0x80000.Isn't it

wrong?

In application program on bank0 i didn't configure fmi registers.

I wait your answers.

Regards...