cancel
Showing results for 
Search instead for 
Did you mean: 

Available Uarts

gdavis
Associate
Posted on February 09, 2006 at 07:20

Available Uarts

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
gdavis
Associate
Posted on February 08, 2006 at 12:40

Hi there, I am new to using the STR710FZ2 and I am just sorting out the hardware connections of the available serial ports. My design requires 2 SPI ports and 4 UARTs, However, I see that the BSPI0 MISO & MOSI pins are shared with UART3 Tx & Rx pins. Does this mean that I can only use one or the other, in which case I think the datasheet should make it clear, as it does with one SPI being multiplexed with an I2C interface.

Thanks in advance