cancel
Showing results for 
Search instead for 
Did you mean: 

Any low limit for MCLK during normal operation

ao-patrick
Associate II
Posted on April 17, 2006 at 07:06

Any low limit for MCLK during normal operation

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ao-patrick
Associate II
Posted on April 13, 2006 at 00:36

In reference manaul version 7 on page 39, it stated as 'There is no lower limit for MCLK. However, some peripherals can show incorrect operation when the system clock has a too low frequency.' So what's the 'some peripherals' means? What kind of 'incorrect operation' will come up?

Because when I configure the MCLK to work on 1MHz, it seems I can not redownload my new code to flash, except that I change the RCCU register values in ICE manually so as to make it work on faster frequency. Besides, when configured as working in 1MHz, the current consumption is 30% lower compared with the value on datasheet. So is there any idea about this?

[ This message was edited by: patrick_jiang on 13-04-2006 04:07 ]