2008-11-01 10:21 AM
[ANN] eLua (Lua for microcontrollers) 0.5 released
2011-05-17 12:56 AM
Hi,
eLua is an open source effort to bring the Lua programming language in the embedded world (MCUs). It is meant to be a complete MCU development environment. It currently runs on a number of ARM variants (STR912FAW44 included), as well as Cortex (and i386 as a proof of concept). Version 0.5 was just released, this is the changelog: * Added support for STR7 CPUs from ST * Added TCP/IP support using the uIP stack * Added support for console and shell over TCP/IP instead of serial link * Added the ''net'' module (eLua's interface to TCP/IP functions) * Added the ''cpu'' module (eLua's interface to the target CPU) * New samples: morse.lua (Morse code encoder), lhttpd.lua (Lua scripting HTTP server) * Added support for cross-compiling Lua code (compile on PC, run on target) * XMODEM can now receive Lua bytecode in addition to Lua source code * The XMODEM buffer is now dynamic (grows as needed) instead of fixed size * Project documentation updated For more details visit the project web page at Best, BogdanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.