cancel
Showing results for 
Search instead for 
Did you mean: 

ADC temperature conversion

user
Associate II
Posted on September 08, 2003 at 11:39

ADC temperature conversion

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
user
Associate II
Posted on September 05, 2003 at 17:01

Hi to all,

can you send me some example about ADC temperature conversion

with 10bit ? To reduce space I have thought to use a 256 step temperature conversion table (255=100° 0=0°) ,

not 1024. Is possible ?

Many tanks to all

mbks
itsmejatinus
Associate II
Posted on September 08, 2003 at 11:39

I think selecting the range will depend up on your type of thermistor you are using. It is because you may have variation of more than 255 steps when the tempreture will rise from 0-100 degrees because of large change of resistance of thermistance so the input voltage with tempreture.