cancel
Showing results for 
Search instead for 
Did you mean: 

ADC speed in fast trigger mode

thomasklatte9
Associate
Posted on October 28, 2008 at 10:30

ADC speed in fast trigger mode

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
thomasklatte9
Associate
Posted on May 17, 2011 at 09:56

I need to run the A/D converter in maximum conversion speed. Im using a new Keil MCB-STR9 board, Processor STR912FAW44 Revision H. Fast trigger in single mode should give 1.2 Msps. Activating the ACG bit in SCU->GPIOANA for fast trigger gives just a little acceleration. I’m polling the ECV Flag and don’t use DMA or interrupt. That might be a problem? After 1000 results, I’m toggle GPIO0 for indication. Im reaching 761 Ksps, if ADC prescaler is set to 0x01. PCLK is 48Mhz. That means ADC Clk is 48 Mhz, too much ! Maximum is 25 Mhz. But reducing ADC Clk reducing conversion rate again.

Can anyone help ?

SCU->GPIOANA |= 0x100; // set ACG-Bit to enable fast trigger mode

ADC->CR |= 0x0002; // POR=1 Power on mode

for (i=0; i

ADC->CR &= 0xFFF7; // STB=0 analog Block is kept powerded on

waitUs_v (50); // wait 50µs.

SCU->GPIOANA |= 0x100; // set ACG-Bit to enable fast trigger mode

ADC->CCR = 0x03; // Config ADC Input Channel 0

ADC->PRS = 0x01; // should be 0x02 !!! fADC = PCLK/2. PCLK=48Mhz, fADC max = 25Mhz.

ADC->CR2 = 0x07; // External Trigger Pin // 0x06; Trigger enabled. Trigger source = External pin

ADC->CR |= 0x8000; //clear ECV

i=0;

toggle = 0;

while (1)

if (ADC->CR&0x8000) { // 0x8000 conversion ready (ECV=1) ?

ADC->CR |= 0x8000; // clear ECV

wert = ADC->DR0; // dummy read

if (++i == 1000) {

i=0;

if (toggle)

GPIO_Write(GPIO0, 0xff), toggle=0; // toggle for diagnostic

else

GPIO_Write(GPIO0, 0x00), toggle=1;

}

}