cancel
Showing results for 
Search instead for 
Did you mean: 

About SMP100LC

UsernameA
Associate

Hi Team,

 

It appears that the varistor turned on at a voltage lower than the value specified in the datasheet.

・​Detailed V-I characteristics of the varistor

・​How significant is the variation between individual varistors?

・Once a varistor turns on, does it remain on even after the power is turned off?

・What is the tolerance of VBO?​

・Does the failure mode of this varistor result in a short circuit?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
FGUIT
ST Employee

Hi,

VBO specified on the datasheet is a maximum value, so it is normal to get a turn ON voltage lower than VBO specified on datasheet (note that VBO is measured according to figure 16 and 17 schematics). Turn ON voltage is between VR value and VBO value.

Regarding SMP100LC turn OFF: once SMP100LC turns ON, the only way to turn it OFF is to reduce the current below IH value.

SMP100LC typically fails in short-circuit when absolute maximum ratings are exceeded.

Best regards.

Fabrice.

View solution in original post

2 REPLIES 2
FGUIT
ST Employee

Hi,

VBO specified on the datasheet is a maximum value, so it is normal to get a turn ON voltage lower than VBO specified on datasheet (note that VBO is measured according to figure 16 and 17 schematics). Turn ON voltage is between VR value and VBO value.

Regarding SMP100LC turn OFF: once SMP100LC turns ON, the only way to turn it OFF is to reduce the current below IH value.

SMP100LC typically fails in short-circuit when absolute maximum ratings are exceeded.

Best regards.

Fabrice.

UsernameA
Associate

Hello, Team,

Thank you for your response.
I understand the contents.

Sincerely,