cancel
Showing results for 
Search instead for 
Did you mean: 

3.5'', 4.3'' and 7'' TFT LCD Module with Touch & MCU interface!

sales23
Associate II
Posted on October 21, 2011 at 10:04

3.5'', 4.3'' and 7'' TFT LCD modules with Touch Panel & LCD Controller (such as K350QVG-V1-F / K350QVG-V2-F) are provided. They have true TFT LCD colors and 8-bit/16-bit 8080 system or 3-wire/4-wire SPI interface and can directly communicate with Microcontrollers. Also, they have perfect performance, reasonable price and they are very popular in the world!

For example, one of Kitronix TFT LCD Modules (3.5'' TFT LCD module with touch panel: K350QVG-V1-F) is used in TI/ Luminary Micro's Reference Design Kits: RDK-IDK-SBC. You can find it at the website:

http://www.ti.com/lit/ug/spmu056c/spmu056c.pdf

http://www.luminarymicro.com/products/rdk-idm-l35.html.

http://www.luminarymicro.com/products/rdk-idm-l35.html.

There are many resources including hardware and software on the website, which can shorten your new products' period.

Also, for more information about Kitronix Display's products, please visit the following website:

http://kitronixdisplay.en.ecplaza.net/

With best regards!

Jacky Sheng

Kitronix Display (H.K.) Limited

Tel:

+86-189-2939-0669

E-mail:

mailto:jacky_sheng@126.com

http://kitronixdisplay.en.ecplaza.net/

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
inaguezz
Associate
Posted on August 11, 2014 at 23:54