2017-03-31 2:23 PM
Hi All,
I just got a SPC560 minimodule and a SPC56XX EVB motherboard. I find the getting started extremely vague. I got the serial cable and I have a serial/usb dongle to connect to my PC.
My questions are,
- what is the best method to flash let's say ChibiOS into the board?
- would it be via CAN? (I don't have JTAG yet).
- Is there any specific terminal program to work with? or should I do it via SPC5Programmer?
I have requested licenses for ST SPC5FlashProgrammer and SPCConnectExplorer but I have not received any answer with the Serial Number yet. What is the expected waiting time? How long that license last for?
2017-04-03 1:45 AM
Hello ,
Did you have SPC5-UDESTK Token ?
Easiest and fastest way.
if yes ,
There is Application example inside Chibios + SPC560B Example (Generate and Compile)
Install it and the driver associated
if not ,
Could you give me your Serial/Usb Dongle name that you use ?
Best regards
Erwan
2017-04-03 11:08 AM
Hi Erwan,
Thanks for your answer.
No, I don't have a SPC5-UDESTK token yet. I ordered it but didn't receive it yet.
I don't understand why would you need the dongle name but it is Keyspan serial/usb dongle.
regards,
Jorge
2017-04-03 11:11 AM
Also, requested last Friday activation keys for SPC5FlashProgrammer and SPC5ConnectExplorer through the installation wizard. I haven't received any email or confirmation or serial or anything. What is the normal process?