2017-02-14 7:41 AM
My project on the P44L3 runs in RUN1 mode and uses SPCSetRunMode(SPC5_RUNMODE_HALT0) in the idle loop for power saving. The PIT timer runs at 1Khz, so switching to HALT0 mode is typically done 1000 times per second.
In some cases - not sure yet how to reproduce though - the SPCSetRunMode() function does not return, but keeps spinning in the for() loop waiting for I_IMODE or I_IMTC, neither of which ever go high. ME.IS is still 0 in this case.
Are there any known circumstances in which this can happen, or anything I could do to debug this issue?
Thank you,
Solved! Go to Solution.
2017-02-26 2:19 AM
For future reference: here is a document from NXP with extensive explanation and solutions:
http://www.nxp.com/assets/documents/data/en/engineering-bulletins/EB770.pdf
2017-02-14 10:15 AM
Further investigation shows that S_MTRANS does not switch to 1 after the sequence
ME.MCTL.R = SPC5_ME_MCTL_MODE(mode) | SPC5_ME_MCTL_KEY;
ME.MCTL.R = SPC5_ME_MCTL_MODE(mode) | SPC5_ME_MCTL_KEY_INV;is executed.
No wonder the for() loop never terminates, as the mode switch has not been performed.
I'm however not able to find out *why* the switching failed. The ME registers have the following values right after the switch instructions are executed:
ME IS:00000000
GS:401F00F4
IMTS:00000000
DMTS:00000000
ME:000005FD
To be continued
2017-02-14 1:39 PM
Might or might not be related: I incidentally see the machine check IVOR1 happen when doing power saving to HALT0. MCSR machine check syndrom register is then set to 0x08000010, meaning 'bus error on instruction read'.
2017-02-15 1:17 PM
It seems that I was hit by two different issues, I'd appreciate any feedback to prove my theory right or wrong:
2017-02-16 12:25 AM
Hello Gert ,
Sorry , for my late answer
Point 2) isright .. it is linked to CFLASH
That's why , you should create some function in SRAM
similar example in STANDBY mode and create your own ld file(user.ld) (note your backupramsection)
i am creating a Change request to add an application example in App Wizard section SPC5Studio
__attribute__ ((section ('.codeinram'))) void gotoStandbyMode(void) {
WKUP.WISR.R = 0x00000008;//Clear interrupt flag
if ((ME.GS.B.S_CURRENTMODE < SPC5_RUNMODE_RUN3)
|| (ME.GS.B.S_CURRENTMODE > SPC5_RUNMODE_RUN0)) {
if (OSAL_FAILED == halSPCSetRunMode(SPC5_RUNMODE_STANDBY)) {
SPC5_CLOCK_FAILURE_HOOK();
}
}
}
__attribute__ ((section ('.codeinram'))) void gotoRunMode(void)
{
if (OSAL_FAILED == halSPCSetRunMode(SPC5_RUNMODE_DRUN)) {
SPC5_CLOCK_FAILURE_HOOK();
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
/*
SPC5 HAL - Copyright (C) 2013 STMicroelectronics
Licensed under the Apache License, Version 2.0 (the 'License');
you may not use this file except in compliance with the License.
You may obtain a copy of the License at
https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.apache.org%2Flicenses%2FLICENSE-2.0
Unless required by applicable law or agreed to in writing, software
distributed under the License is distributed on an 'AS IS' BASIS,
WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
See the License for the specific language governing permissions and
limitations under the License.
*/
/*
* This file is automatically generated and can be overwritten, do no change
* this file manually.
*/
/*
* SPC560Dxx memory setup.
*/
__irq_stack_size__ = 0;
__process_stack_size__ = 2048;
MEMORY
{
flash : org = 0x00000000, len = 256k
dataflash : org = 0x00800000, len = 64k
ram : org = 0x40000000, len = 10k
backupram : org = 0x40002800, len = 2k
}
ENTRY(_reset_address)
/*
* Derived constants.
*/
__flash_size__ = LENGTH(flash);
__flash_start__ = ORIGIN(flash);
__flash_end__ = ORIGIN(flash) + LENGTH(flash);
__ram_size__ = LENGTH(ram);
__ram_start__ = ORIGIN(ram);
__ram_end__ = ORIGIN(ram) + LENGTH(ram);
__backupram_size__ = LENGTH(backupram);
__backupram_start__ = ORIGIN(backupram);
__backupram_end__ = ORIGIN(backupram) + LENGTH(backupram);
SECTIONS
{
. = ORIGIN(flash);
.boot0 : ALIGN(16) SUBALIGN(16)
{
. += 0x00000000;
KEEP(*(.boot))
KEEP(*(.handlers))
KEEP(*(.crt0))
} > flash
.boot1 : ALIGN(16) SUBALIGN(16)
{
/* The vectors table requires a 2kB alignment.*/
. = ALIGN(0x800);
KEEP(*(.vectors))
/* The IVPR register requires a 4kB alignment.*/
. = ALIGN(0x1000);
__ivpr_base__ = .;
KEEP(*(.ivors))
} > flash
constructors : ALIGN(4) SUBALIGN(4)
{
PROVIDE(__init_array_start = .);
KEEP(*(SORT(.init_array.*)))
KEEP(*(.init_array))
PROVIDE(__init_array_end = .);
} > flash
destructors : ALIGN(4) SUBALIGN(4)
{
PROVIDE(__fini_array_start = .);
KEEP(*(.fini_array))
KEEP(*(SORT(.fini_array.*)))
PROVIDE(__fini_array_end = .);
} > flash
.text_vle : ALIGN(16) SUBALIGN(16)
{
*(.text_vle)
*(.text_vle.*)
*(.gnu.linkonce.t_vle.*)
} > flash
.text : ALIGN(16) SUBALIGN(16)
{
*(.text)
*(.text.*)
*(.gnu.linkonce.t.*)
} > flash
.rodata : ALIGN(16) SUBALIGN(16)
{
*(.glue_7t)
*(.glue_7)
*(.gcc*)
*(.rodata)
*(.rodata.*)
*(.rodata1)
} > flash
.sdata2 : ALIGN(16) SUBALIGN(16)
{
__sdata2_start__ = . + 0x8000;
*(.sdata2)
*(.sdata2.*)
*(.gnu.linkonce.s2.*)
*(.sbss2)
*(.sbss2.*)
*(.gnu.linkonce.sb2.*)
} > flash
.eh_frame_hdr :
{
*(.eh_frame_hdr)
} > flash
.eh_frame : ONLY_IF_RO
{
*(.eh_frame)
} > flash
.romdata : ALIGN(16) SUBALIGN(16)
{
__romdata_start__ = .;
} > flash
.stacks : ALIGN(16) SUBALIGN(16)
{
. = ALIGN(8);
__irq_stack_base__ = .;
. += __irq_stack_size__;
. = ALIGN(8);
__irq_stack_end__ = .;
__process_stack_base__ = .;
__main_thread_stack_base__ = .;
. += __process_stack_size__;
. = ALIGN(8);
__process_stack_end__ = .;
__main_thread_stack_end__ = .;
} > ram
.data : AT(__romdata_start__)
{
. = ALIGN(4);
__data_start__ = .;
*(.data)
*(.data.*)
*(.codeinram)
*(.gnu.linkonce.d.*)
__sdata_start__ = . + 0x8000;
*(.sdata)
*(.sdata.*)
*(.gnu.linkonce.s.*)
__data_end__ = .;
} > ram
.sbss :
{
__bss_start__ = .;
*(.sbss)
*(.sbss.*)
*(.gnu.linkonce.sb.*)
*(.scommon)
} > ram
.bss :
{
*(.bss)
*(.bss.*)
*(.gnu.linkonce.b.*)
*(COMMON)
__bss_end__ = .;
} > ram
.standbyram : ALIGN(16) SUBALIGN(16)
{
__standbyram_start__ = .;
*(.standbyram)
*(.standbyram.*)
__standbyram_end__ = .;
} > backupram
__heap_base__ = __bss_end__;
__heap_end__ = __ram_end__;
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Best regards
Erwan
2017-02-16 5:45 AM
Hello Geirt ,
For point 1)
you are right
/* it is recommended to poll S_MTRANS after requesting */
/* STOP, HALT or STANDBY modes */
while(1 == ME.GS.B.S_MTRANS)
{
}�?�?�?�?�?
i am creating an ER for this for RLA & HAL
Best regards
Erwan
2017-02-26 2:19 AM
For future reference: here is a document from NXP with extensive explanation and solutions:
http://www.nxp.com/assets/documents/data/en/engineering-bulletins/EB770.pdf
2017-02-27 12:52 AM
Hello Gert ,
Application Notes for MPC56 (NXP-Freescale) are valid for SPC56 (ST Microlectronics)
Same core
Best Regards
Erwan