2017-06-14 2:52 AM
Hello,
Under certain circumstances involving high interrupt load the CPU triggers a checkstop reset, RGM_FES is 0x8008 in after reboot, indicating the F_CHECKSTOP bit is set.
How do I debug the source of the checkstop reset?
My plan was to disable checkstop reset by setting FERD.D_CHECKSTOP to 1, and then read out MCSR with the debugger when the CPU hits checkstop state. t seems that FERD.D_CHECKSTOP is read only though, so I have no way to disable the checkstop reset.
What would be the best way to debug the checkstop reason, and how can I inspect the value of MCSR before the CPU is forced through a reset?
2017-06-14 6:50 AM
Hello Gert ,
Maybe you can enable FCCU. (cf Chapter 30)
Check chapter 30.7.9 for the Fault mapping
Best regards
Erwan