missing-QuestionPost

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC synchronization problem.

I have ADC synchronized with PWM and it saves data to buffer. PWM is set to be stopped at debugging. It works well until stop at breakpoint.​When I debug program and start from breakpoint, the ADC generates incorrect sequence.How can I fix it?Can I s...

ADian by Associate
  • 628 Views
  • 4 replies
  • 0 kudos

JTAG ID for SPC560B50L5?

Hello thereI want to test my software if its working well, to do so I want to know what is the correct JTAG ID number for SPC560B50L5?I am reading the 0x07C1C01D value from the TDO pin of microcontroller after loading the 0x2 as RS[0:6] in OCMD, is t...

sdrad by Associate II
  • 746 Views
  • 3 replies
  • 0 kudos

I am working on SPC582B and I wanted to use SARADC wizard but when I want to generate SPC5STUDIO application or build the project an error message appear

I am working on SPC582B and I wanted to use SARADC wizard but when I want to generate SPC5STUDIO application or build the project the following message appear Error: Problems opening file: 'L/SPC582Bxx_RLA SARADC Test Application for Discovery/config...

Tilt correction LIS3MDL

Hello?Could you tell me if it is possible to perform a tilt correction on the LIS3MDL.Is it necessary to add an IMU of type MPU6050 or another?Cordially

GPAYS by Associate
  • 267 Views
  • 0 replies
  • 0 kudos

LPS25HB abnormal temperature reading

Hello;I now test the LPS25HB pressure sensor with abnormal temperature reading. The actual ambient temperature is 30 degrees, but the read-out data TEMP_OUT_H (2CH) = DAH, TEMP_OUT_L = 50H. Slowly changing the ambient temperature, temperature reading...

wmeng by Associate
  • 365 Views
  • 0 replies
  • 0 kudos

Unable to connect to SPC570S-DISP once I launch UDE 4.10

I'm trying to use one of the example programs to prove out the connections. Unfortunately, the UDE is not seeing my board. I've not made any changes to the code, simply complied and then loaded debug.wsx in the UDE tool.I had this working before, but...