cancel
Showing results for 
Search instead for 
Did you mean: 

Why does the latest firmware 3.4.3 has only the Demos SD Logging as the only option?

Sudhir
Associate III

I have the latest version of the ST BLE Sensor on Android 9. I changed the firmware to test out the Cube samples. I can't go back to the Pro mode now!!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Sudhir
Associate III

Thanks. I was able to get it to work with the new firmware. The issue may have been that the SD card was slightly out and the software would not come of the SD logging mode.

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @Sudhir​ ,

that's strange, all the firmware version allow the logging on SD card, stream on Bluetooth and on USB/UART.

You could try the last firmware version (you can find it attached to my post) and check if it works.

Please let me know if any issues since this is a new beta version. This is the one with the bootloader, so you should use the STM32CubeProgrammer to upload it (here is described how to do it).

-Eleon

Sudhir
Associate III

Thanks. I was able to get it to work with the new firmware. The issue may have been that the SD card was slightly out and the software would not come of the SD logging mode.