Skip to main content
f87
Associate II
January 22, 2019
Question

Which the difference btw FSM and embedded feature for tap event detection in LSM6DSO?

  • January 22, 2019
  • 1 reply
  • 612 views

Hi, I’m using the embedded tap feature in LSM6DSO. While reading the datasheet, I noticed that it’s possible to implement a finite state machine for the tap activity recognition. Which the advantages, if any?

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    January 22, 2019

    Hi Fingolfin, the FSM approach is quite a different implementation compared to the embedded (single/double) tap.

    The main difference is that the embedded function uses the slope between two consecutive acceleration samples to detect tap events, while the FSM implementation uses the accelerometer raw data directly (without applying any kind of filtering). Moreover, the two implementation might also differs in terms of thresholds, ODRs, timing, etc…

    There are at least a couple of advantages using FSM: in this way, you operates directly on the raw data (e.g. no needs to implement internal filters). Moreover, you can implement up to 16 FSM for tap recognition (different threshold, etc). Also note that the minimum recommended axl ODR for the is 417Hz, while the FSM can work also at lower ODRs (e.g. 26Hz), saving lot of power consumption.

    Let me know if you need any examples.