cancel
Showing results for 
Search instead for 
Did you mean: 

What size of O-Ring and bore hole would you recommend for mounting the ILPS28QSW sensor wather tight?

SBroc.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
allard.potma
Associate II

See documentation for the lps28dfw, application note: AN5937

AN5937 indeed has the dimensions for the o-ring (see Fig. 3).  1.8mm inner diameter, 0.5mm cross-section diameter.

But here's a snag: the smallest standard cross-section diameter is 1mm (from these tables). 

Who makes the appropriate non-standard o-rings?  Please post the suppliers and the part numbers.