Skip to main content
Evelina CAMILLERI
ST Employee
July 8, 2020
Solved

What other hardware can be used as a target for AlgoBuilder GUI?

  • July 8, 2020
  • 1 reply
  • 883 views

[webinar - Program decision trees in sensors with a Machine Learning Core]

    This topic has been closed for replies.
    Best answer by Evelina CAMILLERI

    Except for the SensorTile.box, NUCLEO-F401RE, NUCLEO-L476RG with expansion boards X-NUCLEO-IKS01A2 or X-NUCLEO-IKS01A3 and SensorTile are directly supported in AlgoBuilder.

    A custom HW can be also used. For custom hardware it is necessary to create an AlgoBuilder firmware template using STM32CubeMX and X-CUBE-ALGOBUILD extension.

    1 reply

    Evelina CAMILLERI
    Evelina CAMILLERIAuthorBest answer
    ST Employee
    July 8, 2020

    Except for the SensorTile.box, NUCLEO-F401RE, NUCLEO-L476RG with expansion boards X-NUCLEO-IKS01A2 or X-NUCLEO-IKS01A3 and SensorTile are directly supported in AlgoBuilder.

    A custom HW can be also used. For custom hardware it is necessary to create an AlgoBuilder firmware template using STM32CubeMX and X-CUBE-ALGOBUILD extension.