cancel
Showing results for 
Search instead for 
Did you mean: 

What is the actual design of the accelerometer low pass filter?

lasersocks
Associate II

I am attempting to use the LPF2 chain on the LSM6 accelerometers. The cut-off frequency is described as something like ODR_XL/100. I assume that means if you are running at 12.5 Hz the cutoff frequency is then .125 Hz. I am assuming that this is the 3 dB cutoff of the filter? I am still getting mechanical noise to make its way into the accelerometer response, so I am wondering what the actual design of the filter is. Is it just a single pole filter? Basically just a moving average of a 100 samples. Or is it a multi pole filter? and if so how many poles?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TSand.1
Associate III

Hi @lasersocks​ , ya, probably the LPF2 is a single pole filter (-3dB the cutoff), since it is only defined by this frequency. But I let ST to validate this hypothesis.

/tim

View solution in original post

2 REPLIES 2
TSand.1
Associate III

Hi @lasersocks​ , ya, probably the LPF2 is a single pole filter (-3dB the cutoff), since it is only defined by this frequency. But I let ST to validate this hypothesis.

/tim

Hi @TSand.1​ , @lasersocks​ ,

that's correct.

-Eleon