cancel
Showing results for 
Search instead for 
Did you mean: 

What is clock frequency of finite state machine located on the MEMS sensor?

Evelina CAMILLERI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Considering the clock frequency in this question as the rate the FSM processes data, there are four available data rates in LSM6DSOX: 12.5 Hz, 26 Hz, 52 Hz, 104 Hz.

The FSM data rate can be chosen in Unico-GUI when building the FSM, or alternatively configured through the FSM_ODR1 and FSM_ODR0 bits in the EMB_FUNC_ODR_CFG_B (5Fh) register of the LSM6DSOX.

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Considering the clock frequency in this question as the rate the FSM processes data, there are four available data rates in LSM6DSOX: 12.5 Hz, 26 Hz, 52 Hz, 104 Hz.

The FSM data rate can be chosen in Unico-GUI when building the FSM, or alternatively configured through the FSM_ODR1 and FSM_ODR0 bits in the EMB_FUNC_ODR_CFG_B (5Fh) register of the LSM6DSOX.