2020-09-17 8:59 AM
This is quite urgent!
Solved! Go to Solution.
2020-09-24 8:46 AM
Hi Dale,
Thank you for your appreciated feedback.
Yes, please consider that the important timings for the self test are described in the lsm6ds3_self_test.c (and in the AN4889 app note) and are the following ones:
#define BOOT_TIME 20 //ms
#define WAIT_TIME_A 200 //ms
#define WAIT_TIME_G_01 800 //ms
#define WAIT_TIME_G_02 60 //ms>> I also heard a rumor that something changed in the firmware in the LSM6DS3. Is that true?
Well, I can't know if you changed something in your firmware... ;) But I suggest to check the last fix on Github, if it is aligned with your fw.
-Eleon
2020-09-24 8:53 AM
2020-09-24 9:00 AM
We may refer to different things, I suppose. I believe you built up your custom application, composed by an application processor + a LSM6DS3USTR. I'm referring to the firmware / software that is running on your application processor, and in particular to the part dedicated to check Self test check in production. No changes inside the electronics of the sensor, from ST side.
Please let me know if I misunderstood your point.
-Eleon
2020-09-24 9:16 AM
2020-09-24 9:19 AM
understood... could you please ask your team if they can send you (and then to me) two pictures of the top package marking of the LSM6DS3s, one of a good sample and the other one of a failed sample? There are some tracking information on it.
Thanks
-Eleon
2020-09-28 12:23 AM
Hi @DGree.6 ,
Please let me know if you eventually managed your issue, or in case if we can give further suggestions to you.
-Eleon
2020-09-28 2:27 AM