Skip to main content
TBurd.1
Visitor II
July 27, 2022
Question

Very rarely happens that LSM6DS3 doesn't change state on INT2 pin while new data is available. Is possible that is freezed and only power on reset helps? Config: 0x12, 0x01) 0x12, 0x24) 0x10, 0x48) 0x13, 0x80) 0x11, 0x4C) 0x0D, 0x01) 0x0E, 0x01)

  • July 27, 2022
  • 1 reply
  • 687 views

..

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    July 29, 2022

    Hi @TBurd.1​ ,

    Are you facing the same issue also configuring the INT1 pin instead of the INT2?

    Can you also try to latch the interrupt (LIR bit of the TAP_CFG (58h) register)?

    You might also compare your code with a C examples on Github like --> lsm6ds3_tap_single.c

    -Eleon