2025-12-05 8:06 PM
Hello ST Team,
We are using the STEVAL-MKI109V3 as the motherboard and STEVAL-MKI208V1K (IIS3DWB vibration sensor) as the daughter board.
We currently communicate using the USB virtual COM port at 115200 baud and send ASCII commands such as:
*SETDB208V1
*ZOFF
*W10A2
*DEBUG
*STOP
These commands work correctly over USB.
Objective:
We would like to print the data serially using the same commands, but over Bluetooth, not USB.
The accessory board STEVAL-MKI115V1 is no longer available in the market.
We tried using an HC-05 Bluetooth UART module, connecting it to BT_TX and BT_RX (J9 connector), but it did not work, so the default MKI109V3 firmware support UART input/output on the BT_TX / BT_RX pins ?
Any guidance or documentation regarding alternative UART usage or supported alternative Bluetooth modules would be greatly appreciated.
Thank you.
Raj