2021-09-10 6:32 AM
I need to use a gyroscope with my Nucleo-64 board, but the gyroscope needs to stand apart (i.e. at the end of a cable). Is the STEVAL-MKI197V1 a good match? Can I connect it directly to my Nucleao-64 with a SPI cable, *without* using an expansion board? (such as X-NUCLEO-IKS01A1, X-NUCLEO-IKS01A2, X-NUCLEO-IKS01A3, X-NUCLEO-IKS02A1).
Solved! Go to Solution.
2021-09-10 7:13 AM
Hello @paul19
Yes there is no problem to connect it through cables instead of the easy plugin Arduino connector.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-10 7:13 AM
Hello @paul19
Yes there is no problem to connect it through cables instead of the easy plugin Arduino connector.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-18 8:13 AM
Thanks @Bruno_ST. It works well indeed.
For reference, the SPI connection can be found here.