cancel
Showing results for 
Search instead for 
Did you mean: 

Use case: a pressure sensor which acts as an altimeter. At a place where there is a wide season change,does the LPS27HHTW provide the accuracy as mentioned in the Data sheet?My use case has critical implications and need an accuracy of about +1m (.12hPa).

AVarg.6
Associate

Does it also give the mentioned accuracy during weather changes? (Use case is set up in Europe.)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Uwe Bonnes
Chief

The datasheet only carries typical values, so no accuracy is guaranteed at all...