cancel
Showing results for 
Search instead for 
Did you mean: 

USART communication INEMO- STM32F4

sinatra
Associate
Posted on May 02, 2015 at 13:38

Good morning guys. I'm writing because I need help for interfacing an Inemo M1 with a STM32F4. I have the need to take all the sensor values of  Inemo on  F4 via USART. I used to start the sample code of  'Inemo called ''AHRS_LIB_Continuos'' and I implemented a small library for port configuration USART1 that I post below:

#include ''inemo_usart_interface.h''

#include ''iNemo_Led.h''

/* PIN on J12 equal to Tx 6 (GPIOA9) e Rx 7 (GPIOA10)*/

FlagStatus xUsartTxComplete;

FlagStatus xUsartRxComplete;

void usart1_IRQHandler(void);

ErrorStatus usart_initialize() {

  

  USART_InitTypeDef usart_init;

  NVIC_InitTypeDef NVIC_InitStructure;

  GPIO_InitTypeDef GPIO_InitStructure;

  

  /*Enable usart periph clock */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1, ENABLE);

  

  /* Configure and enable usart1 interrupt */

  NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

  NVIC_Init(&NVIC_InitStructure);

  

  /* Configure usart pins: RX and TX ---------------------------------*/

  /* Configure MISO pin as Alternate Function Push Pull */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  

  /* Init usart */  

  usart_init.USART_BaudRate = 512000;

  usart_init.USART_WordLength = USART_WordLength_8b   ; 

  usart_init.USART_StopBits = USART_StopBits_1;

  usart_init.USART_Parity = USART_Parity_No;

  usart_init.USART_Mode = USART_Mode_Rx;

  usart_init.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_Init(USART1, &usart_init);

  

  USART_Cmd(USART1, ENABLE);

  

  USART_ITConfig(USART1, USART_IT_TXE, ENABLE);

  USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);

  xUsartRxComplete = USART_GetFlagStatus(USART1, USART_IT_RXNE);

  xUsartTxComplete = USART_GetFlagStatus(USART1, USART_IT_TXE);

  iNEMO_Led_Toggle(LED1);

  return SUCCESS;

}

void usart_raw_receive(uint8_t *data, uint16_t length) {

  

  uint16_t i;

  uint8_t rxbyte;

  

  for(i=0; i<length; i++) {

    rxbyte = USART_ReceiveData(USART1);

    data[i] = rxbyte;

    while(xUsartRxComplete != SET);

    xUsartRxComplete = RESET;

  }

  

//  if(data[0] == 0xAA){iNEMO_Led_Toggle(LED1);};

}

void USART1_IRQHandler(void) {

  if (USART_GetITStatus(USART1, USART_IT_TXE) != RESET) {

    xUsartTxComplete = SET;

    USART_ClearITPendingBit(USART1, USART_IT_TXE);

  } else if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) {

    xUsartRxComplete = SET;

    USART_ClearITPendingBit(USART1, USART_IT_RXNE);

  }

}

  

Given that the transmission from the F4 working properly, because already tested, I need to run the rx and tx on 'Inemo. Do you believe that I have to change something in the example code (for example vector table or other things ) and in my library? In particular in this case I'm trying to send a byte from F4 to inemo to test the communication, but it doesn' t work.

Thank you. I await answers.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0