2025-09-01 11:17 PM
After turning on the gyro and accelerometer with the CTRL1_XL and CTRL2_G registers of the ASM330LHH, if the TDA bit in the STATUS_REG does not change to 1 (XLDA and GDA are set to 1), is it effective as a countermeasure to cause the TDA bit to change to 1to turn off the gyro and accelerometer with the CTRL1_XL and CTRL2_G registers and then turn on both sensors again?