cancel
Showing results for 
Search instead for 
Did you mean: 

SensorTile Datalog to SD cannot reach 500 Hz?

JWu.3
Associate

I am using STSW-STLKT01_V2.1.1 package Datalog project to program the sensortile. It works perfectly at 200Hz logging acc+ gyro+ Magnetometer data. I disabled all other sensors. However, if I increase the logging frequency to 500 Hz, it work for 5 seconds and shut down automatically. Does anybody know why?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @JWu.3​ , please consider that a new FW version (2.2.0) is available, you can try with this revision if the issue is solved. Btw, please note that the STSW-STLKT01 package is not optimized to manage higher rates than default, differently from newer platforms such as the STWINKT1, whose data-logging and data management in general is optimized for every ODR. Regards