2020-05-11 5:58 AM
2020-05-12 11:20 PM
Yes it is possible, but you have to change IKS01A3 communication from default I2C to SPI (for the DIL24 socket at IKS01A3), then connection of STEVAL-MKI208V1K is possible. Currently there is no out of the box SW project published to suport this combination of HW, but there are many source codes available which could be adapted. For example to look at X-CUBE-MEMS1 SW package as starting point for IKS01A3 in general.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.