cancel
Showing results for 
Search instead for 
Did you mean: 

Quaternions in AlgoBuilder with sensortile box

LRoss.1
Associate

Hi everyone,

I'm using the quaternions and the sensor fusion in Algobuilder with the Sensortile box in order to compare the signal of the quaternions and the position of the teapot, but I don't understand the relation between both of them... Any idea?

When I turn the Sensortile box 90° in X-axis, the teapot turns -90°.... WHY???

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
RMcCa
Senior II

"Conpare the signal of the quaternions And the position of the teapot"

When did Lewis Carroll start writing code?​