cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSR RMS Noise

adrianT
Associate II

Hi,

We are evaluating the LSM6DSR's noise floor for a specific use case. Based from the datasheet the noise is 60ug/sqrt(hz). 

So calculating the RMS noise at 208Hz should result to 0.00062 m/s^2 right? However, we are getting measured RMS values around 0.002 to 0.004 m/s^2.

 

Here are some configurations set

FS: +-2G

ODR: 208Hz

Data acquired using FIFO reading every 500 samples

No onboard filtering enabled.

 

I have attached a sample dataset for your analysis as well.

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @adrianT ,

60×106×9.80665=0.0005884m/s2/Hz

Considering a BW of 104Hz (ODR/2) -> 0.0005884×104=0.0005884×10.198=0.006m/s2

Your calculation of 0.00062 m/s² seems to be off by a factor of 10, the correct RMS noise from datasheet noise density at 208 Hz ODR should be approximately 0.006 m/s².

Your measured RMS noise values of about 0.004 m/s² are acceptable.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @adrianT ,

60×106×9.80665=0.0005884m/s2/Hz

Considering a BW of 104Hz (ODR/2) -> 0.0005884×104=0.0005884×10.198=0.006m/s2

Your calculation of 0.00062 m/s² seems to be off by a factor of 10, the correct RMS noise from datasheet noise density at 208 Hz ODR should be approximately 0.006 m/s².

Your measured RMS noise values of about 0.004 m/s² are acceptable.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.