cancel
Showing results for 
Search instead for 
Did you mean: 

lsm6dsl AWT interrupt

ABran.4
Associate II

hello

i use STEVAL-MKI178V2 (adapter board) + STEVAL-MKI109V3 (motherboard) with UNICO-GUI ver9.13.

i try "Absolute wrist tilt" example as it described in "AN5040 - Rev 3".

The questions are:

- in "A_WRIST_TILT_Mask (59h)" register, each bit by itself works fine. but if i use more than 1 axis (x and y, or y and z) - i got continuous interrupts (interrupt than latency time than interrupt ...). see attached picture

- in "A_WRIST_TILT_Mask (59h)" register, for each axis i got absolutely same behavior for positive and negative tilt.

please advice

Alexander

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0