LIS3DH reading axes values problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-01-05 10:42 PM
Posted on January 06, 2016 at 07:42
I'm using LIS3DH_driver project from ST to read axes values from LIS3DH accelerometer.
I'm not using STM32 but I have implemented my own LIS3DH_ReadReg() and LIS3DH_WriteReg() functions somehow and they are working without a problem since I can write and read back registers correctly. But the problem is when I call LIS3DH_GetAccAxesRaw() function to retrieve axes values and print them out I don't see a correct value and they are not changing when I hit the accelerometer by thumb and they're really high values even when the board (or the IC) is not moving at all (when I'm not clicking). I have enabled FIFO mode and data rate is 50HZ and WHO_AM_I is 0x33 which is correct I believe. I have not configured any interrupt pins cause I don't need it's functionality. I couldn't figure this out by myself. Anybody have an idea?
Labels:
- Labels:
-
Accelerometers
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0