cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH Low-power mode

LM
Associate II

LIS3DH MEMS digital output motion sensor.

Hi every body.

I'm using this sensor in 'High-resolution mode'. but after some time (I define timeout = 10 seconds) without detect any motion, put the sensor in 'low-power mode'. if the sensor is moved before this 'timeout' (detect interrupt), change to 'High-resolution mode'.

this works as expected,

but, when the 'Low-power mode' is set (after timeout), the sensor is sending an unexpected interrupt, this is producing than my software detect the interrupt, so, is returning to 'High-resolution mode'.

resume: every time the sensor is set to 'Low-power mode', it is returning an interrupt. the interrupt need to be just when the sensor detect motion.

any help?

thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

HI @LM​ , are you using the sleep-to-wake-up and return-to-sleep functions of LIS3DH? I mean the one described in p. 23 of AN3308. Regards