cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH datasheet error?

Mich1
Associate III
Posted on December 16, 2013 at 14:53

In LIS3DH datasheet (Doc ID 17530)

on table 25 we can see: Default value 00     ODR3-0 (0000:50Hz Others:...)

on table 26 we can see: 0000 Power down mode

So what is ODR = 0000  Power down or 50Hz?

#lis3dh
1 REPLY 1
bw
Associate II
Posted on February 19, 2014 at 12:09

Hi,

ODR = 0000 is power down, this is confirmed in Applicaiton note AN3308.

My experience is that the application notes are the most reason updated.