cancel
Showing results for 
Search instead for 
Did you mean: 

LIS344ALH Vibration Rectification

damon kutten
Associate II
Posted on March 15, 2018 at 17:24

Hello,

Do you have any information about Vibration Rectification Error (VRE) on the LIS344ALH (2g setting)? 

Specifically, I am driving the device into saturation. During and following the saturation, I am seeing what appears to be a significant DC offset on the output. This offset eventually decays, as long as the device is not forced back into saturation.

Has the behavior of the device been characterized when it enters saturation, especially if saturation is asymmetric in the presence of gravity?

Thanks,

                              Damon

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on March 19, 2018 at 15:03

We do not measure this characteristic.