cancel
Showing results for 
Search instead for 
Did you mean: 

Is there limitation for SPI address auto-increment option in LIS3MDL devices?

Zip
Associate

Hi All,

I can read successfully in burst mode "MS bit is set to '1'" the data from output registers X_L, X_H, Y_L,Y_H,Z_L and Z_H.

But if i add temperature data TEMP_OUT_L, TEMP_OUT_H into read frame the temperature value is not read.

Examples:

Rx buffer after reading 9 bytes, start adress = 0x28 "OUT_X_L"

dummy ; X_L ; X_H ; Y_L ; Y_H ; Z_L ; Z_H ; X_L ; X_H

Rx buffer after reading 15 bytes, start adress = 0x28 "OUT_X_L"

dummy ; X_L ; X_H ; Y_L ; Y_H ; Z_L ; Z_H ; X_L ; X_H ; Y_L ; Y_H ; Z_L ; Z_H ; X_L ; X_H

It seems like auto-increment register address option work only for magnetometer data and when reached adress 0x2D "Z_H" then is reset to 0x28 X_L for next read.

Could some one confirm this behavior. Or did I overlook something in datasheet ;)

Have a nice day.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee

Yes, I can confirm it is, it is standard behavior.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.