cancel
Showing results for 
Search instead for 
Did you mean: 

Is CTRL_REG0 on LIS3DH available since the beginning?

luisf
Associate II
Posted on February 23, 2017 at 02:39

Hi, I have a project that uses LIS3DH. I just noticed an update at the Datasheet and now there is a  CTRL_REG0 that I can disable the SA0 pull-up. Is this available since the beginning or just on new batches of the device?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Miroslav BATEK
ST Employee
Posted on February 23, 2017 at 09:14

It is available since the beginning.

luisf
Associate II
Posted on April 25, 2017 at 21:51

Thank you. Is there any special procedure or timig restriction to disable the pull-up? I am using the LIS3DH with the SPI and i see some current leakage with the pull-up? Sometimes i send the command and the current goes away and sometimes it dont.